Other Parts Discussed in Thread: TUSB3410
Hi,
We are using the Texas Instrument driver TUSB3410 with our XL50 product – our XL50 product uses the TI chip and has two ports, a serial port and a USB (2.0) port. I have written a terminal emulator program which communicates to the DB9 serial port and also to the USB port, well except when the user pulls the USB cable out of the XL50. In this case, the TUSB3410 driver which we installed from the TI web site is removed from the Device Manager and the terminal emulator’s memory is “internally” corrupted due to buffer over-run. Other times, the driver and the terminal emulator work fine and memory leak detections program do not detect any leaks. We are running this under Win 7 but our clients could use WinXP or Win7 (32 or 64). Is there a configuration on the driver side to have Windows 7 not remove the driver when the USB cable is unplugged?
Thanks,
Bahram