This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[Q] SN75DP130DS power dissipation



Dear TI-er.

I check the SN75DP130DS EVM power dissipation.

3.3V: 156mA -> 515mW

1.05V: 116mA -> 122mw

Total Power: 637mW

Why it different in Datasheet page 10 ?

I want know Power Supply test conditions.

Plz help me.

  • Hello elsalvador,

        The test conditions for typical and maximum values are the following:

    Typical:

           Temperature:   Room temperature (25 Celsius degrees)

           Voltage:              Nominal values (VCC= 3.3V & VDDD= 1.05V)

    Maximum:

           Temperature:   Maximum (85 Celsius degrees)

           Voltage:              Maximum values (VCC= 3.6V & VDDD= 1.2V)

    Best regards,

    Diego.