Other Parts Discussed in Thread: LMH1983
Hi all.
There is a question of LMH1983.
To the table of Audio FORMAT detection code, It is checking that four sorts of word clocks are published.
To Support Format Lookup Table of Table.1 Since only two sorts were published, it checked.
Are they four sorts of 32k,44.1k,48k,96kHz? (Word clock)
At the time of a word clock input, Although the signal was outputted TOF2 and TOF3, TOF1 did not output.
Is it normal now? (Three TOF are made a setup of output enabling. )
In addition.
There is a question about the HOLDOVER operation at the time of a reference input being lost.
In resister 05h is 2Bh (default) and 18h is 01h (default) and 19h is FFh (default),
Although the 1Ah is 00h (default) and 1Bh is 01 h (default) oparate it,
In this state, when a reference input is lost, it goes into HOLDOVER operation,
The error output voltage of PLL1 should keep the error output voltage at the time of there being a reference input.
However, error voltage will not be kept if actual operation on an evaluation board cuts the input of a reference,
It will change on unfixed voltage.
Why doesn't it carry out normal HOLDOVER operation?
Best Regerds,
Hisa Kobayashi.