This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1310A - Errata RX.Detect Fail

Guru 19785 points


Hi.

Our customer is having trouble can not recover from P3.

Could you please tell us in detail about the errata, "RX.Detect fails in P3" ?

I am understanding that one should use PIPE Power State in P2 instead of P3 when RX.Detect fails in P3.

But, normally I think the USB device receives the LGO_U2 or LGO_U3 packet from the host, then set the power state.

In this workaround, do you mean that you ignore the LGO_U3 packet and choose P2 power state ?

Best Regards,
Kawai