Other Parts Discussed in Thread: TUSB3410
Hi,
Sometimes, the USB driver unloads and when attempting to disable/enable device from Device Manager, it causes the computer to blue screen and reboot. Other times, when the host computer restarts, it says that one of the USB devices attached to this computer has malfunctioned and Windows does not recognized it. Under USB Root Hub (3 ports), the Generic USB Hub sub device which has a exclamation icon is called "Unknown Device". Disabling and re-enabling this does not fix the problem and causes blue screen of death to appear. The driver is working intermittently. I am currently writing this post from that computer and this is exactly when the problem has occurred, i need to reboot and try to see if disabling the COM port at the BIOS will affect the behavior.
Thank you,
Bahram