Other Parts Discussed in Thread: LMH0366, LMH0341
Is it possible to disable the reclocking of the loopthrough? If not, how is the behavior of the loopthrough when the input is at 125Mbps (MADI)?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LNIC
The LMH0341 is a deserializer which only deserializes data at 270Mbps, 1.5Gbps or 3 Gbps. It will not operate with MADI. If you need a reclocker that will operate at MADI rates, please look into the LMH0366 which is a dedicated reclocker, which supports MADI rates as well as standard broadcast video rates