Other Parts Discussed in Thread: SN65LVDS4
Hello.
I am having difficulty with an AC coupled LVDS system composed of a SN65LVDS105PW driver and a SN65LVDS4 receiver.
The circuit is constructed as recommended in the "AC-Coupling Between Differential LVPECL, LVDS, HSTL, and CML" guide, http://www.ti.com/lit/an/scaa059c/scaa059c.pdf page 7 figure 11.
The issue arrises when I attempt to send a square wave through the system with non-50% duty cycle (10MHZ < Fs < 100MHZ). Specifically, the pulse width skew is significantly higher than specified in either part's respective datasheet. At 50%, the low going prop delay and the high going prop delay (measured from single ended input of 105PW to single ended output of LVDS4) are very well matched, however, at duty cycles other than 50%, there is significant prop delay mismatch, which manifests as pulse width fidelity problems from input to output. An additional oddity is that at high duty cycles, the low going prop delay is much shorter that the high going prop delay (> 2ns difference), whereas at low duty cycles, the behavior reverses and the high going delay is shorter than the low going delay.
Can anyone tell me what is going on? Is this expected behavior? Can I restructure the circuit to enable Tplh=Tphl at any duty cycle?
Thank you in advance!