Problem Description : Device Vendor’s ID and Device ID are read properly but, read and write to the device is not working.
Snapshot of the different control and data signals are in attached file for memory write. Data snapshot is only for last four bit of data (LSB).
In my design TI PCI Bridge 2050BIZHK is used. The design is based on MPC 8548E processor on Integrity 5011 RTOS. The block diagram of configuration is described in attached file. In this design MPC 8548E is used as a processor and PCI Bridge is used to connect the PCI slave on other board via motherboard. PCI Bridge is connected on PCI 2 bus on primary side of processor.
My PCI slave is not hot swappable. Do i need to follow any power on sequence such as P_VCCP and S_VCCP be powered up first before applying power to VCC?
The bridge (2050B) configuration details are also attached in word document.
Please advice.
Thanks in advance