Other Parts Discussed in Thread: TFP401
hello there,
i used the tfp401 to build a display-demonstrator for customer presentations. the board has an eeprom with edid information on it and worked perfectly for now.
The new display I had to attach has a 480x240 resolution and a PCLK of 8.2 MHz within a range of at least 6 and not more than 13 MHz.
The question is if I can drive the display with this chip? i read about the 2 pixel/clock modus of the tfp which can drive a PCLK of 12.5 MHz which would meet my requirements. I routed the QE outputs only and I don't get a nice picture on the display though I measured a PCLK of 12.5 MHz on the display input. Is it possible to do that or is it worth a try?
thank you for your help