Other Parts Discussed in Thread: DS80PCI800
Hello,
can you recommend the redriver settings: de-emphasis, equalizer, signal detect threshold level for the system which consist of the PC riser card with DS80PCI800 chips, external PCIe cable 1m length, DUT card with also DS80PCI800 chips. Gen.3 link, width is x8. What additional information need to know that to set proper mode of the de-emphasis ,equalizer etc.
In datasheet, for example, for de-emphasis settings there are information for trace 20inch max. What should be settings when the cable 1m is present?
Thanks.
Alex