Other Parts Discussed in Thread: DP83848I-MAU-EK
Hi Everyone,
The AN-1469 PHYTER Design & Layout Guide says that the MII IEEE spec states that the bus should be 68 Ohms. In the next section in the guide goes on to recommend series termination resistors of 50Ω on the PHY to MAC MII lines. Wouldn't the optimal resistor be 68Ω for these termination resistors? Also, since the design guide calls out 50Ω resistors, is it implying that 50Ω transmission lines are acceptable. With MII running over a short distance to the MAC, say a few inches, wouldn't the transmission lines effects on the digital lines(excluding clock lines) be irrelevant to proper operation since the signals would all settle before any sampling occurred? Since the clock lines are going from the PHY to the MAC, then if the transmission line to MAC interface are matched, would that work adequately too (ignoring the output impedance on the actual PHY)?