Can I use the RS-422 driver 26C31 in combination with the receiver AM26LV32 without problems?
This because I need to use a part with the 26C31 build in.
And on the otherside i need to interface to a 3,3V FPGA LVTTL input
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can I use the RS-422 driver 26C31 in combination with the receiver AM26LV32 without problems?
This because I need to use a part with the 26C31 build in.
And on the otherside i need to interface to a 3,3V FPGA LVTTL input
Willem,
Yes, this is possible. The connection is RS422 driver with a RS422 receiver.