Other Parts Discussed in Thread: ULN2003LV
Hi all.
ULN2003LV is used, please let me know the following.
Can an internal transistor present the input voltage (OFF voltage) which serves as OFF certainly?
Please give me the minimum including individual variation and temperature variation.
When it cannot describe above, The graph which the OFF characteristic understands is available
Conditions: an output current of 3.5 mA~13 mA, ambient air temperature -20 ℃~70 ℃
Best Regards,
Hisakichi Kobayashi.