This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83640 MDIO pull-up resistor

Hi

The datasheet specifies a 1.5k pull-up resistor at the MDIO pin. Is it very important to use this exact value or would e.g. 2.21k also be okay? Is it possible to specify a tolerance for the required pull-up resistor.

Thanks in advance for feedback.

  • Carsten,

    IEEE 802.3 specifies the pull-up resistor for MDIO as 1.5 kOhm +/- 5% for applications in which the PHY is attached via the MII cable described in the spec.  The value of 1.5 kOhm was chosen to allow several PHYs to be bused together, i.e. to share the MDC and MDIO signals. 

    The overwhelming majority of implementations that I see these days connect MDC and MDIO in a point to point fashion between the PHY and the MAC.  In these cases, strict adherence to the specification is not required.  A 2.2 kOhm resistor with a tolerance of +/- 10% should be sufficient.

    Patrick