This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH0346 - Unused Output

Guru 19785 points

Other Parts Discussed in Thread: LMH0346

Hi,

Please let me ask you what is the best way to do with the unused output of LMH0346, +/-SCO/SDO2 pin (Pin14,15).

It was good if the device had disable function for each channel, but it can only enable or disable both output at the same time.

Shoud we just connect 100ohm termination resistor between Pin14 and15 ? 

We want to minimize the influence to the main signal SDO1.

* There is an app note enabling SMBus access, but our customer will use in Pin mode only.

Best Regards,
Kawai