Hi,
Is there an LVDS mux in 2:1, 4:1 or 8:1 format which can support LVDS Back Channel.
I want to mux 8 LVDS Cameras to one Output Display, but also have LVDS Back Channel comms from the Display.
Thanks,
Liam
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Is there an LVDS mux in 2:1, 4:1 or 8:1 format which can support LVDS Back Channel.
I want to mux 8 LVDS Cameras to one Output Display, but also have LVDS Back Channel comms from the Display.
Thanks,
Liam
Hello Liam,
Yes, TI does offer several LVDS mux devices that would accomodate the backchannel. These include a 2:1 mux function. Here are a few suggestions.
http://www.ti.com/lit/ds/symlink/hd3ss3412.pdf
http://www.ti.com/lit/ds/symlink/hd3ss213.pdf
Best regards,
Sue
Hi Sue,
Do you know of any 4:1 or 8:1 mux with same capabilities? LVDS and Back Channel
Thanks,
Liam
Hi Liam,
Unfortunately at this time i am not aware of such a part(i.e 4:1 mux).
Could you please tell us about the application and perhaps a block diagram?
Regards,,nasser