Other Parts Discussed in Thread: ISO721
By reading ISO 13849-2, I found in table D.19 requirements suitable for optocouplers. However both ISO 13849 and IEC 61508 do not mention requirements for any other digital isolator. In my project I would like to use a gavanic isolator like ISO721 or similar, to isolate a SPI interface between a safety uC and another regular uC.
For optocouplers, the standards require that the device must be built in accordance with overvoltage category III and polution degree 2, as described in IEC 60664-1. Does it applies for galvanic isolators too? is that possible to use ISO721 or similar in safety applications?
Thanks in advance.