Other Parts Discussed in Thread: TFP401, DS92LV2421, TFP410, SN75LVDS83B, SN65LVDS93A
Dear,,,
I designed TFP401+DS92LV2421 --> DS92LV2422-->TFP410. It works.
TFP410/410 can run up tp 165Mhz. However, Ser-Des can run up to 75Mhz.
75Mhz can cover upto 1024 x 768 @60Hz....
Is this the maximum Resolution?
If any ser-des which can support the speed as TFP401 (165Mhz), please let me know.
Best Regards,
P.S. I have to transmit the DVI signal on a single core of the optical fiber.