This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TFP401+DS92LV2421 --> DS92LV2422-->TFP410

Other Parts Discussed in Thread: TFP401, DS92LV2421, TFP410

Dear,,,

I designed TFP401+DS92LV2421 --> DS92LV2422-->TFP410. It works.

TFP410/410 can run up tp 165Mhz. However, Ser-Des can run up to 75Mhz.

75Mhz can cover upto 1024 x 768 @60Hz....

Is this the maximum Resolution?

If any ser-des which can support the speed as TFP401 (165Mhz), please let me know.

Best Regards,

P.S. I have to transmit the DVI signal on a single core of the optical fiber.