Other Parts Discussed in Thread: TCA9517
TCA9517 data sheet (page 2/21) stated that
"Because of the buffered low voltage from the B side, the TCA9517 cannot be connected B side to B side and to ensure clock-stretching support the B side should not be connected to a device with rise time accelerators."
Question 1
Please refer to the attached file on the I2C interface.
Is it ok to use TCA9517 as level shifter to interface with only 1 of the 3 devices, and the other 2 devices are directly interfaced to DM368 (as I2C master)?
(All the 3 devices can support fast mode up to 400kbps)
Question 2
From the link below:
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/100/p/227663/800566.aspx
Renjith is saying that "I don't think it's possible to do I2C clock stretching in DM36x."
In this case, can DM368 still work with TCA9517 without clock stretching support on the B side?
Or is there a need of clock stretching implementation for SCL up to 400 kHz max?
Kindly enlighten
Regards