Other Parts Discussed in Thread: TLK10232, ONET8501PB
Hi: What is the input RX sensitivity of the TLK10232 for a BERThis thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TLK10232, ONET8501PB
Hi: What is the input RX sensitivity of the TLK10232 for a BERHi David,
I am a little bit confused on your question, could you please elaborate?
In the data sheet is states that the minimum voltage that can be received by the TLK10232 by the HS and LS receivers is 50mV differential. Does that answer your question or am I off base on this?
Regards,
Mike
Mike:
Thanks for answering but the question i'm posing is not to find out what the minimum input differential is, but what is thta voltage for the HS receivers that gives a bit error rate < 10E-12 at 10.3Gb/s for a PRBS31 pattern. All high speed limiting-amps (look at the ONET8501PB limiting amplifier for example) give a voltage spec for this condition.
The ONET8501PB datasheet says that voltage is 5mV typically (see page 5 under Data Input Sensitivity). I need to know the equivalent voltage spec for the TLK10232 tranceiver. The very definition of input sensitivity is that voltage at the input of the limiting amplifier that gives a certain BER (at a defined data rate and pattern) at its output.
Regards,
David
Hi Dave,
We do not have a spec like that for the TLK devices. The ONET8501PB is a post amplifier and it is not the same beast as a SerDes so there is not a comparable spec. The 50mV differential minimum that I pointed out earlier is sort of like the ONET spec because it implies a BER of <10E-12 even though it may not be stated.
In actuality though you can throw a closed eye at the TLK10232 and still achieve a BER of <10E-12 as the device implements a FFE and a DFE on the receive side. These features allow you to take a 10G-KR signal that has a lot of ISI due to backplane traces and/or cables and achieve a BER like you mentioned above.
Please let me know if you have additional questions and I will be glad to help.
Mike
Mike:
If the 50mV differential minimum implies a BER of 10E-12 (and i hope it does), then why is LOS asserted at <75mV?
Are you saying that the TLK10232 could assert LOS but still deliver a BER of 10E-12? Sorry, i'm confused...
David
Hi David,
(I thought I would jump in since Mike is out of the office today.)
Yes, the LOS assert threshold is higher than the minimum input voltage, so it is possible to have a link up and running with LOS asserted. This may seem counter-intuitive, but it can be useful to have some indication of a signal problems before errors actually occur - especially since the device already has mechanisms to indicate bit errors at the receiver.
As Mike pointed out, though, with such a complex receiver it is difficult to have a spec that bounds only one aspect of the input signal. This spec was based on testing that provided a "clean" input eye (from test equipment) with a low input amplitude. If there were significant other impairments (such as random jitter, noise, etc.) present simultaneously, the BER could degrade even if the (nominal) signal level was still above this limit. On the other hand, a low BER can be achieved with a totally closed input eye if the signal impairments are primarily "equalizable" - that is, they result from physical media losses/reflections/etc. that can be compensated by a decision feedback equalizer (DFE). This capability of the device is encompassed by the jitter tolerance specification, which indicates BER < 1e-12 operation in the presence of channel attenuation, additional random and deterministic jitter, and broadband random noise.
Best regards,
Max Robertson
SerDes/PHY Systems Engineer
Texas Instruments
m-robertson@ti.com
· The chip can achieve BER < 1e-12 with an “open” input eye of amplitude greater than or equal to our minimum input voltage spec. In this case, equalization doesn’t really play into it since there isn’t an uneven frequency response to compensate (or else the eye wouldn’t be “open”). In this case, it is possible for LOS to assert even though the link is operating properly.
· The chip can also achieve BER < 1e-12 with a “closed” eye provided that the eye is closed primarily as a result of something equalizable like electrical high-frequency loss. In this case, LOS is unlikely to assert. Most data will have a spectrum that includes low-frequency components as well, and these will not be affected as strongly by media losses. This means that the eye opening may be 0 V (due to high-frequency losses and intersymbol interference) but the peak-to-peak amplitude could still be fairly large.