Other Parts Discussed in Thread: TUSB8040A1
Dear TI!
I'd like to design a special USB 3.0 HUB with the TUSB8040A1.
My problem is, that in some designs I found the RX and TX pair mixed up. I mean the IC's downstream USB_SSRXx_xxx port was connected to the USB connector's TX pin, and the SSTX... to the RX pin.
It is a normal USB 3.0 "A type" female connector and if I swipe the RX and TX at the IC's downstream port and connect the RX pin to the connectors's TX, should it be correct?
Here are 2 designs, which sould be correct? ( the normal has the connector at the bottom, the cross on the top)
https://dl.dropboxusercontent.com/u/126286420/cross.jpg
https://dl.dropboxusercontent.com/u/126286420/normal.jpg
Thanks,
Peter