Other Parts Discussed in Thread: ISO7241C
I have a customer asking the question below:
TI ISO7241C part -
The data sheet states that the part “operates with 3.3V or 5V“. The “Recommend Operation Conditions” table has a note that states:
“For the 5-V operation, VCC1 or VCC2 is specified from 4.5 V to 5.5 V.” This is 5V +/- 10%.
I need to operate the circuit at 4.5V? If I add in any tolerance on that I am outside the range in the datasheet.
Would you please verify that the ISO7241C will work at intermediate Vdd (for example: 4.0V) voltage levels?