Other Parts Discussed in Thread: TFP410
Our customer observed the following symptom.
They have 1080p60 video output to a monitor, it will not show all picture.
The bottom 10 or more horizontal line shows black when connected to a certain monitor.
Customer asks us why this symptom occurs.
They understand that there is an errata of H_RES count < 2047. So they set the registers as the below. *
DE_DLY: 127
DE_CNT:1920
DE_TOP: 41
DE_LIN:1080
* HV total and HV active range are,
H-Total: 2200
H-Active: 1920
V-Total: 1125
V-Active: 1080
Pixel Freq: 148.5MHz (Vfreq: 60Hz)
But they are setting as the below because of the errata.
H-Total: 2047
H-Active: 1920
V-Total: 1125
V-Active: 1080
Pixel Freq: 148.5MHz (Vfreq: 60Hz)
[Question]
Why does this happen ?
[Question]
When setting as the above, is there NO "DE" signal under DE_LIN=1080(Active Video) ?
Best Regards,
Kawai