Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI SN75DP139 support for 4096x2304 resolution

Other Parts Discussed in Thread: SN75DP139

Dear Sir TI SN75DP139 SPEC have show to DP139 can support 4K2K , the 4K2K resolution are 3840x2160 and 4096×2160. But Intel chip provide 4096x2304 resolution , Can we use DP139 for this project?
  • Hello,

    The DP139 will support any resolution with a data rate up to 3.4Gbps, for example a resolution of 4k2k@30Hz has a pixel clock of 297MHz which equates to 2.9Gbps over HDMI.

    So you need to know what is going to be your data-rate.

    Please provide more information about the application and more specifications regarding the DP and TMDS sides.

    Regards.