Other Parts Discussed in Thread: DS64MB201
Hi Team,
Our customer is observing the following symptom.
They have same signal input to SIA0 and SIB0.
When selecting the input using SEL0/1 pin, DOUT0 waveform shape of DE changes in random.
We guessed the Auto Rate function was not working well and asked customer to try setting RATE=Low, but no change.
Why do you think this happen ?
We must understand why and how we can clear this problem.
Please give us your advice.
[Condition]
- Same signal(2.4576Gbps) is input to SIA0 and SIB0
- EQ level for SIA0/SIB0 is set to 9dB (ADR 0x0F,0x16 = 0x30)
- DE level of DOUT0 is set to -6.0dB (ADR 0x18 = 0x88)
---> THIS SYMPTOM DID NOT APPEAR WHEN DEM SET TO " -6dB COMPATIBILITY MODE" (ADR 0x18=0x08)
- RATE pin is set to AUTO (They have also tested in Low(3Gbps mode))
* I could send you customer waveforms offline, could you please give me an Email ?
Best Regards,
Kawai