Other Parts Discussed in Thread: ISO3086T, ISO35T
Hello, all
Now we have one inquiry from our customer who is considering to use ISO3086T or ISO35T.
They have fixed the VCC1 input voltage to 3.3V, however has not fixed the VCC2 input voltage on either of these devices.
Also, they would like to use DA2304 (turns ratio 1:2.2) than DA2303-AL(1:1.5) which seems to be flexible usage on both VCC2=3.3V or VCC2=5V.
In case VCC1=3.3V and VCC2=3.3V for ISO35T, please let us confirm whether the configuration below could be suggested.
VCC1=3.3V => DA2304 => 6V => TPS76333 => 3.3V => VCC2
We thank you in advance for your information.
Best regards,