I have built a new optical detection system with an internal USB 3 hub. The firdst Protoyp is arrived and I have problems with the HUB. IT is working fine with Low Speed and high Speed. Is just can’t use the Super Speed Performance. The PC is only sometime recognize the USB 3 device and informs me that the device can perform with a higher performance. Question: What can cause this behavior . Routing of the TX /RX pairs?