This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75DP139 Sink-TEST

Hi  members.

This is  Ben.
Professor, please.

《The state》
 ・Engineer   examines  DP139   for extension port   for   TV side.
 ・SINK-TEST  ID8-7:jitter-tolerance level.
        2.97Gbps and  2.2275Gbps   is  passed.
        270Mbps is  FAIL.
    It is necessary  for this reason  seek  something.

 《Q1》
 ・Engineer confirmed   oscillator  by  switching ON's swing.
     Engineer  thinks   the  fail reason  transition time a stability of a swing.
     Do you have that this will be reason to the  270Mbps FAIL?

《Q2》
 ・270Mbps is  near jitter frequency level. and  would be margin less.
    Do you have that this will be reason to the 270Mbps FAIL?

 

Best  regard.   
BEN