Other Parts Discussed in Thread: DS26LV32AT, TPA2006D1
Hi, Question :DS26LV32ATM Input Short condition
The input side "RIx+" and "RIx-" If the side is short-circuited, (7-pin and 6-pin short, for example)
Would you have any stress to the device.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DS26LV32AT, TPA2006D1
Hi, Question :DS26LV32ATM Input Short condition
The input side "RIx+" and "RIx-" If the side is short-circuited, (7-pin and 6-pin short, for example)
Would you have any stress to the device.
Hi Cafain,
The inputs of the DS26LV32AT will not be damaged if they are shorted together, as long as the receiver input voltage stays within the absolute maximum ratings (±14V).
In terms of the TPA2006D1, the way I interpret the datasheet is that if the device is in shutdown the VCC pin can take a maximum of 7.0 volts. This is determined by the /SHUTDOWN pin being pulled low or left floating (since there is an internal pull down on the pin). I would confirm this with the audio amplifiers team in the Audio Amplifiers Forum since I have never worked with that device. The link is below:
http://e2e.ti.com/support/amplifiers/audio_amplifiers/f/6.aspx
Thanks,
John
Hi Jone-san
In early reply, I appreciate.
I was helpful to you.
Thanks.
Cafain