Other Parts Discussed in Thread: TLK110, CDCE913, AM3359
Hi,
I refer to the following thread: http://e2e.ti.com/support/interface/ethernet/f/903/t/310855.aspx
There it is written that the TLK110 needs to be strapped to RMII mode and that the clock needs to be 50MHz to be able to switch it to MII mode with register RCSR.
1. Question:
Does the clock has to stay at 50MHz after the switch to MII mode or should it be switched to 25MHz?
2. Question:
We have a board that clocks the PHY with 25MHz during power-up (CDCE913 with 25MHz crystal). The TLK110 is strapped to RMII mode. What we can do is switching the clock from 25MHz to 50MHz after power-up and then switch the TLK110 to MII mode (using register RCSR). Is this possible?
3. Question:
What is the reason to have the clock 50MHz while switching the TLK110 from RMII to MII mode?
4. Question:
What about the transition from MII back to RMII? What is the right way to do that?
It would be very helpful if someone from TI could further clarify the switching procedure and maybe give some background information (e.g. about the clock).
Thanks and best regards,
Patrick