Other Parts Discussed in Thread: TFP501
Please allow me to ask three questions bellow
Q1. If TFP501/501 can be used in HDMI application?.
I think the HDMI and DVI sues the same physical layer called TMDS.
If so, can you use TFP501 In a HDMI source device?
Likewise, can TFP510 be used in HDMI Sink device?
Q2. If TFP510 evaluation board or reference design is available?
Q3. When an on board EDIT ROM is re-programed, do you need to power of the TFP501,
need to keep its power on, or can be re-programmed regardless of power on/off of TFP501?
Mita