Other Parts Discussed in Thread: SN65HVD1780
1) What additional external protection components does TI recommend? We were thinking of using SMA30CA (30V bi-directional 400W TVS). If you see a problem with this (or a better implementation), I would like to hear it. 2) On the datasheet (Absolute Maximum Ratings), what is the difference between the specification for "Voltage range at A and B inputs" and "Voltage input range, transient pulse, A and B, through 100 Ω". The values are identical, aren't these specs redundant?