Other Parts Discussed in Thread: ISO1540, ISO1541
About the ISO1540, I would like to connect the side 1 on the I2C bus, and the side 2 on a device, because the Vil_max of the device is 0.8V, as the maximum Vol of the ISO1540 on side 1.
I've read on the datasheet to connect side 1 on the device, and side 2 on the bus, but in this way the noise margin would be zero, so I couldn't use the ISO1540.
I would like to know if I can swap the two side, and if there are some adverse side effects.
Thanks,
Aurelia