This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Deselializer for DS90C185

Guru 20090 points

Other Parts Discussed in Thread: DS90C185, DS90CR288A, DS90CR287, DS90CF386, DS90CR218A, DS90CR286A, DS90CF366

Hello,
 
Are there the deserializer which pair of DS90C185 ?
Our customer request the device which has below specifications.
I bilieve DS90C185 can use as transmitter(serializer).
However  I can't find the receiver(deserializer ).
 
<specifications>-------------------------------------------------------------------
-Vdd=1.8V
- IO Voltage=1.8V
-16bitYUV ~ 24bitRGB
-Receiver integrated Equalizer
-DCLK Frequency above 80MHz
-Low power comsumption : Tx + RX < 200mW
 ---------------------------------------------------------------------------------------
 
Best Regards,
Ryuji Asaka
 
  • Ryuji-San,

    There are two options:

    1). They can consider DS90CR287 and DS90CR288A. These two are pair of ser/des used by other customers for 28 bits 85MHz applications.

    2). They can also consider DS90C185 with DS90CF386.

    Regards,,nasser

  • Hi,

     

    You can use any generation 1 FPD-Link, Channel Link or Flatlink deserializer with the DS90C185.

     

    This includes the:

    • DS90CR288A
    • DS90CR218A
    • DS90CR286A
    • DS90CF386
    • DS90CF366

     

    Most of these 7:1 LVDS deserializer type devices have been incorporated into the timing controller (TCON) for the disaply panels. This IP is also widely available from all major FPGA vendors.

     

    Mike Wolfe

    DPS APPS / SVA