Other Parts Discussed in Thread: PCF8575, TCA9535
Hi
I am using PCF8575 for driving MOC3603 OPTOCOUPLER .
When use the PCF8575 without driving the optocoupler, the output on the IO's of PCF8575 is 4.5V when driving the outputs high.
When I connect the PCF8575 outputs to the optocoupler through a 390 ohm resistor and drive the output high the output of the PCF8575 is 1V.
Vf of the input led of the MOC3606 optocoupler is 1.2V , so the current sinked from the port is (5V-1.2)/390=9.74mA
May you kindly tell me what is wrong with my calculations and design and how to solve the problem
Attached you can find schematic for my circuit
Regards
Hossam Alzomor