Other Parts Discussed in Thread: TSB12LV32-EP
I am working on a project using the TSB12LV32-EP Link Layer Controller (LLC). I would like to simulate signal integrity on the LLC's Microcontroller Interface. Ideally I would like an IBIS model to cover the Microcontroller Interface pins (primarily BCLK, MD[0:15], MA[0:6], MCAn, MCSn, MWRn). Can anyone advise if this is available or, alternatively, if a different TI IBIS model can be used with equivalent IO buffers? Alternatively, can anyone advise output rise/fall time on these pins? (the input rise/fall time is specified in the datasheet).
Thanks, Richard.