Other Parts Discussed in Thread: DP83640SW-LIB
Hi!
I'm trying to set the GPIO1 as PPS output. Can I get a detailed algorithm for this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DP83640SW-LIB
Hi!
I'm trying to set the GPIO1 as PPS output. Can I get a detailed algorithm for this?
The best starting point for this will be the Software Development Guide (SDG) and the EPL C code reference library. These are avialable on-line at:
http://www.ti.com/tool/dp83640sw-lib
The SDG will include descriptions of the functionality beyond what is in the datasheet. The EPL C code reference library will provide C code examples of various functionality.
Patrick
Thanks!
I read these instructions and tried to follow it, but there is no pps.
My actions:
SetPHYPage(PHY_PG4_PTP_TSTS, ethNumber);
unsigned short reg = (0 << P640_TRIG_SEL_SHIFT) | P640_TRIG_DIS;
PHYWrite(reg, PHY_PG4_PTP_CTL,ethNumber);
PTPSetTriggerConfig(ethNumber, 0, P640_TRIG_PER|P640_TRIG_PULSE|P640_TRIG_NOTIFY , 1);
PTPArmTrigger(ethNumber, 0, 5, 0, false, false, 500000000, 500000000);
SetPHYPage(PHY_PG4_PTP_TSTS, ethNumber);
tstPhy = PHYRead(PHY_PG4_PTP_TSTS,ethNumber);
...tstPhy =0x0002 - error...
Code of functions:
void PTPArmTrigger(unsigned char ethNumber, unsigned short trigger, unsigned int expireTimeSeconds, unsigned int expireTimeNanoSeconds,
bool initialStateFlag, bool waitForRolloverFlag, unsigned int pulseWidth, unsigned int pulseWidth2)
{
unsigned short reg;
SetPHYPage(PHY_PG4_PTP_CTL, ethNumber);
reg = (trigger << P640_TRIG_SEL_SHIFT) | P640_TRIG_LOAD;
PHYWrite(reg, PHY_PG4_PTP_CTL,ethNumber);
PHYWrite(expireTimeNanoSeconds & 0xFFFF, PHY_PG4_PTP_TDR,ethNumber);
reg = (expireTimeNanoSeconds >> 16) | (initialStateFlag ? 0x80000000 : 0) |
(waitForRolloverFlag ? 0x40000000 : 0);
PHYWrite(reg, PHY_PG4_PTP_TDR,ethNumber);
PHYWrite(expireTimeSeconds & 0xFFFF, PHY_PG4_PTP_TDR,ethNumber);
PHYWrite(expireTimeSeconds >> 16, PHY_PG4_PTP_TDR,ethNumber);
PHYWrite(pulseWidth & 0xFFFF, PHY_PG4_PTP_TDR,ethNumber);
PHYWrite(pulseWidth >> 16, PHY_PG4_PTP_TDR,ethNumber);
if ( trigger <= 1)
{
PHYWrite(pulseWidth2 & 0xFFFF, PHY_PG4_PTP_TDR,ethNumber);
PHYWrite(pulseWidth2 >> 16, PHY_PG4_PTP_TDR,ethNumber);
}
reg = (trigger << P640_TRIG_SEL_SHIFT) | P640_TRIG_EN;
PHYWrite(reg, PHY_PG4_PTP_CTL,ethNumber);
}
//****************************************************************************
void PTPSetTriggerConfig(unsigned char ethNumber, unsigned short trigger, unsigned short triggerBehavior, unsigned short gpioConnection)
{
unsigned short reg = 0;
if ( triggerBehavior & P640_TRIG_PULSE) reg |= P640_TRIG_PULSE;
if ( triggerBehavior & P640_TRIG_PER) reg |= P640_TRIG_PER;
if ( triggerBehavior & P640_TRIG_IF_LATE) reg |= P640_TRIG_IF_LATE;
if ( triggerBehavior & P640_TRIG_NOTIFY) reg |= P640_TRIG_NOTIFY;
if ( triggerBehavior & P640_TRIG_TOGGLE) reg |= P640_TRIG_TOGGLE;
reg |= gpioConnection << P640_TRIG_GPIO_SHIFT;
reg |= trigger << P640_TRIG_CSEL_SHIFT;
reg |= P640_TRIG_WR;
SetPHYPage(PHY_PG5_PTP_TRIG, ethNumber);
PHYWrite(reg, PHY_PG5_PTP_TRIG,ethNumber);
}
A PPS is a periodic trigger with a 1 second period. There are some notes on this in section 3.1.4.6 of the SDG.
There is an example configuration of a PPS using Trigger 0 shown in section 3.2. There is also an example configuration in the ptpControl.c file.
Patrick