Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Powering switched capacitor RS232 devices from separate supply?

Other Parts Discussed in Thread: MAX3243E

Hi, I want to put in about 25 MAX3243E chips in a design, but I don't want to power the RS232 interface by the on-board switched capacitor scheme. Can I attach a separate (central) supply to the +V and -V pins (presumably +6V and -6V DC) and leave out the switched capacitor circuit capacitors? (Obviously, needing a few general bypass caps here and there). Is there an application note for this? I think I saw this suggested somewhere before, but I can't find it. Thank You, Joe Norris

  • Joe,

    You need to make sure that at no time VCC > V+ or V- > GND. Reason: internal diode VCC to V+ and V- to GND
    C1 and C2 pins must be unconnected.

    I am not aware of an application note, but I have used this method internally for MAX3xxx device testing.
    In summary the idea is technically feasible, but I do not have full characterization data to support this.