Other Parts Discussed in Thread: SN65LV1023A, DS92LV18, DS92LV16, DS92LV2422, DS92LV2421, DS15EA101, DS15BA101, TLK2711-SP, SN75LVDT1422, DS99R103, DS99R104
Dear all,
I have a question regarding SN65LV1023A power supply. Normally if we make an ADC interface circuit, the analog and digital supply needs to be really separated so that the one doesn't interfere with the others. However, I saw something interesting in the datasheet that states "DVCC and AVCC are separated internally and does not matter what the difference is for |DVCC−AVCC|, as long as both are within 3 V to 3.6 V".
So I wonder if the difference doesn't matter, can I just use a same source separated by beads for the analog and digital supply? Or should I use a really isolated power supply like when we deal with ADC circuits?
I attached an image here to make sure that my intentions are clear:
Thanks for your attention. Looking forward to hearing something.
Cheers,
Fajar