Other Parts Discussed in Thread: LMH0030, LMH0031
I have applied all the voltages properly. The IO pin 6 is giving 3.3V as it is supposed to be, but other than that there's absolute no response. I have verified all the connections. Applied 27Mhz at the Ext clk. Made sure the proper initialization of power i.e. 2.5v is applied after 3.3v. The Control register write flow is working for LMH0030, but LMH0031 is not responding in any way at all.