Other Parts Discussed in Thread: XIO3130
Dear Expert
There are some issue in our customer.
Could you please advice for issue ?
condition
CPU : Intel BayTrail-IE3845 1.91GHz Quad Core
OS : Windows Embedded 64bit
XIO3130 is connected to the ch3 of PCIE
ch1 and ch2 of XIO3130 is connected to the Spartan6 of Xillinx.
ch3 is opened because of unused.
They have tested and approved for use SandyBridge as extention board of FPGA.
They use the tool that is "Read&Write Utility" to test connection PCI devices.
There are 2 kinds of issue.
Issue 1
The device connected to ch1 cannot be accessed.
Clk is output during 2~2.4msec after startup , and then clk is stopped.
When ch1 is removed connection, clk is output 1msec ,and then clk is stopped immediately.
Issue 2
FPGA device connected ch2 has 3 area of memory and FPGA use BAR1,BAR3 and BAR4.
Although FPGA can access to BAR1 and BAR3 , FPGA can not access but can read only "0".
Best Regards