Other Parts Discussed in Thread: TUSB9261
What is the TUSB9261 Maximum power consumption on VDD 1.1V?
Data sheet states 291 mA typical but give no maximum.
Will a 500mA regulator be sufficient?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TUSB9261
What is the TUSB9261 Maximum power consumption on VDD 1.1V?
Data sheet states 291 mA typical but give no maximum.
Will a 500mA regulator be sufficient?
Thanks
Hello Joel,
The maximum power consumption of the TUSB9261 on VDD11 is close to 291mA (it depends on many factors however you can use this value as valid reference), so the 500 mA regulator is OK as long as it is used only for VDD11.
Regards,
Diego.