This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS442 / GND separation of HDMI

Guru 29720 points

Other Parts Discussed in Thread: TMDS442

Hi team,
 
My customer is considering TMDS442 for adoption.
He designs peripheral circuit of the device and concirned if it is necessary to separate each GND of DDC/CEC(17pin), TMDS Data Shield(2,5,8,11pin), FG(outer periphery of connector and chassis).
 
Is there any recommendation of GND separation with TMDS442?
This isn't pure question of the device(TMDS42), so I think it may be difficult to answer...but I'm glad if you give me a comment.
I also heard that there is competitive device that GND separation is recommended.
 
Best Regards,
Yaita / Japan disty
  • Hello Yaita-san,

    You don't need to separate the ground for those pins, what needs to be isolated are the different voltage rails, for example VCC_IO, VCC_PLL, etc.

    When using connectors, it is recommended to connect the connector chassis to the power ground through a filter to reduce EMI (like the picture below)

    You can find more information about PCB Design guidelines here http://www.ti.com/lit/an/scaa082/scaa082.pdf