Other Parts Discussed in Thread: DS15BR400, DP83620, DP83620-EVK, DP83849IF, DP83849IFVS-EVK
Hi everyone,
I have an in-house built optical transmitter (LED) and ROSA (PIN & TIA) that we are developing as our optical link. I would like to demo this link by building a prototype 100Mbps Ethernet - Optical and Optical - 100Mbps Ethernet media converter.
My question is, what kind of 100Mbps Ethernet Transceiver chip is suitable for this purpose based on my transmitter and receiver specification below.
Transmitter - Input Signal : Works best with LVDS. But it will be able to take low voltage differential in the region of 200mVpp to 500 mVpp differential. The common move voltage is not important as I will AC-couple the signal before entering the device.
Receiver - Output signal is SLVS, which is Vcm = 200mV and Vswing = 200mV (single ended). I will use the output in differential mode
My Tx-Rx link can achieve up to 700Mbps using LVDS input signal to my transmitter (I used TI DS15BR400). However, the target of this demo is only at 100Mbps using 100Base-T configuration. Based on my transmitter requirement and receiver output, I think it works best if there is an Ethernet - LVDS transceiver chip, but I'm not sure if TI has such a thing.
I realize that there are many 100Base-T to SFP media converters out there. However, our current transceiver product is still in prototype form and are not in the SFP module form. Thus, I'm looking to purchase the transceiver chip (or its Eval board) and try to tap the signal direct to my transmitter, and also take my receiver's signal to the chip for media conversion.
Thanks in advance!