Other Parts Discussed in Thread: DS64BR111
Hi,
I'd like to ask about the values below of absolute maximum ratings.
・Maximum Package Power Dissipation at 25°C:xxx W
・Derate:xxx mW/°C above +25°C
Is there any value?
Best Regards,
Yaita
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DS64BR111
Hi Yaita,
DS64BR111 Data sheet indicates indicates the package thermal characteristics as Theta JA with maximum junction temperature of 125 Deg C and maximum current consumption of 63mA.
At 63mA and 3.6V supply this means the device maximum power consumption is 234mW. Given this, the maximum operating Junction Temp = 85 Deg C(Max Operating Ambient Temp) + .234X33(Deg C/W) = 92.72 Deg C. This is well within the specified maximum 125 Deg C junction temp.
Regards,,nasser