Other Parts Discussed in Thread: HD3SS3412, HD3SS6126
I have questions for you about HD3SS3412 4ch High performance Differential Switch.
(The application is for factory interface board )
Q1: The HD3SS3412 offers USB3.0 application but does the switch support USB2.0 Full speed voltage range (3.3V)?
It looks that this switch doesn’t support USB2.0 as far as looking at other spec parameter of differential voltage which is max 1.8V at least.
I know that USB3.0 and USB2.0 are different interface from spec wise. (USB spec revision 2(USB2.0)/ USB3.0 spec revision 1(USB3.0))
Q2: What happen with the output voltage from the switch when 3.0V differential voltage (eg. USB2.0 Full speed) is applied as input?