Other Parts Discussed in Thread: SN65HVD234
I'm using the TI SN65HVD234 CAN XCVR which we use on several of our products. I want to use the SLEEP mode for minimum supply current, and the data sheet says that I must set EN to 0 and D to VCC. If there is a voltage on the CAN bus from some other node, will this affect the sleep mode supply current? Currently, the part powers up with RS held at VCC, so I believe that the part is guaranteed to be in the recessive mode until Rs goes below 0.33 Vcc. I've seen no problems with this, but I want to make sure I don't cause one by using the EN pin, which is currently held to Vcc.