Other Parts Discussed in Thread: TUSB2046B
I have laid out a usb hub for a project using the tusb2046b. I mainly based my design off of the reference design labeled figure 11 in the data sheet. When I plug in mass storage devices it says that the max power is exceeded and I would assume thats because of hte current limit of only 100ma per port. It looks like I need to move to a self powered version rather than a bus powered one. Also When I plug in the device (which i'm using now for this keyboard and my mouse) it says that I am limited to usb 1.1 speed. I was under the impression that this usb controller chip was capable of usb 2.0 operation. Is there steps I need to take in order to make it run at usb 2.0 speed or did I choose the wrong IC altogether?