Other Parts Discussed in Thread: TPD2E009
Hi,
I have a question about TPD2E009.
The data sheet is described about system leve ESD(IEC61000-4-2).
Please let met know why device level ESD(HBM/MM/CDM) isn't specified.
Best Regards,
kato
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPD2E009
Hi,
I have a question about TPD2E009.
The data sheet is described about system leve ESD(IEC61000-4-2).
Please let met know why device level ESD(HBM/MM/CDM) isn't specified.
Best Regards,
kato
Kato-san,
Any device that meets IEC61000-4-2 Level 4 specification far exceeds the HBM/MM/CDM highest level ratings of 4000/400/1000 V (respectively) and over similar time intervals. Therefore these standards are not mentioned because they are far exceeded.
Regards,
Yater-san,
Thank you for your response.
There is one more questions that I would like to ask you.
I suppose that IEC61000-4-2(Level 4) is guaranteed Air-Gap Discharge 15kV.
However, the data sheet is described 8kV.
Would you kindly tell me why the data is difference?
Best Regards,
Kato
Kato-san,
Thank you for bringing this discrepency to our attention. Level 4 rating is 15 kV Air Gap, and we do not meet that one. I will add have this data sheet updated. Be aware that process takes many weeks. I apologize for any inconvenience.
Regards,